800XA V6.1 - IEC61850 - CI818 - LN CLASS
Hello,
I have a problem in updating the scd configuration of my IEC61850 CI818 card.
I can't add the energies contained in MMTR LN Class.
I can add all MMX i want but no MMTR.
Have you an idea ?
Do you know if the CI868 manage this class ?

Thanks !
I have a problem in updating the scd configuration of my IEC61850 CI818 card.
I can't add the energies contained in MMTR LN Class.
I can add all MMX i want but no MMTR.
Have you an idea ?
Do you know if the CI868 manage this class ?
Thanks !
Answers
Energy Signals in MMTR Logical Node is not supported by CI868.
It will throw an error like "MMTR/Dmdwh/actVal" ignored from IO Channel creation while importing SCD file. Unsupported type - INT32.
It will throw an error like "MMTR/Dmdwh/actVal" ignored from IO Channel creation while importing SCD file. Unsupported type - INT32.
Add new comment