Missing Toolbox Item in Graphics Builder PG2
Hi.
I would like to build a Graphic Display and use the object BMI_ValueAndUnitInd (ValueAndUnitInd in its 'core'). This object can be found at the Graphics Structure and the Object Type Structure, as show bellow.
But, I could not instantiate this object trough Toolboxes, in Graphics Builder (PG2). The image bellow shows the 'missing' element.
I have tried copying the attributes and details of "StandardOnOffSymbol" and "StandardStdBySymbol", but was unable to use it. I've also tweaked the Object Type Structure, the Graphics and the Library one, but no success.
Despite that, if I create a new Graphics Toolbox Item Type object from scratch, it works.
I would like to/need to use the built-in resources of the system to build this Graphic Display and I'm not allowed to create new stuff in other structures.
Does anyone know how to solve that problem?
Thanks in advance!
Voted best answer
Answers
You should only use the "BMI Core Elements", AnalogValueCore in your case, on Process Displays
Add new comment