Problem installing 800xa 6.0.3-3
I have problems upgrading offline a system from 5.1FP4 to 6.0.3-3. I have now installed(deploy) all the new software and the nodes is added to the SCC showing green.
But there is only in the redundant aspect server where the system notification icon is green and saying that the system is running. In all other nodes the notification icon I red and saying that the system I stopped.
In the service event list you can see that for every other node there is “Aspect Directory Connection refused “nodename”. For connectivity servers the service AdvMbTtdSrv and for clients the service AfwServiceManager is in the message.
Is the system broken or can it be fixed.
Answers
Hello
Couple of things to be clarified
1. Whether clients and Primary server are pinging by both name as well as IP?
Check to the node administration structure whether remote node connection is executing without any error by saying Registration successful.
Make sure network related settings are similar in all nodes.
Under Advance configuration DNS and WINS settings to be made similar for all nodes.
Check with the firewall settings. Firewall to be kept off.
If set up is in domain kindly refer to Domain Configuration settings related to Server manager .
Couple of things to be clarified
1. Whether clients and Primary server are pinging by both name as well as IP?
Check to the node administration structure whether remote node connection is executing without any error by saying Registration successful.
Make sure network related settings are similar in all nodes.
Under Advance configuration DNS and WINS settings to be made similar for all nodes.
Check with the firewall settings. Firewall to be kept off.
If set up is in domain kindly refer to Domain Configuration settings related to Server manager .
Add new comment