How to connect Secondary server with ASCS in Workgroup?
I have one EWS running on 800xA6.1 which is ASCS in Workgrou, and I have another Engineering laptop(800xa6.1 installed which is Client and Domain configured).
Now i want to make this Engg laptop as redundant Connectivity Server of ASCS in Workgroup.
Please suggest the way to do this
Voted best answer
Put short: since 800xA v6.0 it is not supported to move computers between different systems.
Officially supported method: restore the drive image you took before installing System 800xA on the laptop (or reload the Microsoft Windows operating system from scratch).
Officially supported method: restore the drive image you took before installing System 800xA on the laptop (or reload the Microsoft Windows operating system from scratch).
Add new comment