Copy program from one PM573 to another using SD Card?
Can I use any Memory card in PM573 or there is any specific?
What is the maximum capacity of memory card, compatible with PM573 and what file format it should be?
Can you please advise about the "communication Error" as I don't have the TK503 cable, I am connecting directly through the Network cable.
Answers
Hi
to make a copy of the program inside a cpu you can refer to my app at the following link, but I see that you have already downloaded it. So what would your question be? If it concerns the memory card capacity, ABB's standard one is 512 Mb, but I know that some users have used 1 Gb or even 2 Gb , type for photo cameras, without problems.
https://forum-controlsystems.abb.com/...
In reference to your question about the "communication error" it is a very generic description, which could have more and more causes, so try to better explain what happens, perhaps with some photos.
Make sure, first of all, that you have your PC with Automation Builder, on the same domain where you have the CPU, because otherwise this could also be a cause of "communication error"
BR
Flavio
to make a copy of the program inside a cpu you can refer to my app at the following link, but I see that you have already downloaded it. So what would your question be? If it concerns the memory card capacity, ABB's standard one is 512 Mb, but I know that some users have used 1 Gb or even 2 Gb , type for photo cameras, without problems.
https://forum-controlsystems.abb.com/...
In reference to your question about the "communication error" it is a very generic description, which could have more and more causes, so try to better explain what happens, perhaps with some photos.
Make sure, first of all, that you have your PC with Automation Builder, on the same domain where you have the CPU, because otherwise this could also be a cause of "communication error"
BR
Flavio
Add new comment