Repository Login
Hello Every Body,
As you see in attached photo,i tried to login in Engineering Repository ,but cant ;does any one know about how resolve problem?
As you see in attached photo,i tried to login in Engineering Repository ,but cant ;does any one know about how resolve problem?
Voted best answer
Before use, Engineering Repository must be setup as per Appendix A in the System 800xA 6.1 Post Installation, 2PAA111693-610 guide.

For must users, the regular ImportExport tool is a better fit.

For must users, the regular ImportExport tool is a better fit.
by Stefan Stromqvist
Engineering Repository is a lesser used function in System 800xA that can be useful when transferring engineering between a production system and an engineering system. Most users of System 800xA uses ImportExport for this; are you sure you want to use ER instead of the regular ImportExport tool?
First, you must set ER up correctly - what steps have you done to set it up?
by mohsennazari6453 Rank: 433 on 2/2/2021 4:37:04 AM | Like (0) | Report
Acctually i read this feature from doc.no:.3BSE046784-600 page 29,what this mentioned; this has some diffrencies with export import tool for example Engineering Repository allows to defune aspect category filters to prevent aspect ad e.g Operator notes to be overwritten in production systems,etc.so try to open that for controllers object in control structure but isnt.
I had did not any work for set up,i imagined that vendor set up that.what should i do for set up or which document i must read for setup that?
Add new comment