Mapping of ACS580 Drive Current on DCS
Dear i want to map current coming from an AC drive ACS580 to my Freelance PLC, i have scaled my SCALE Input Range from 0-16384 and Range Output 0-17. I am using Motor Current 01.07 Parameter.
The Transmission Media between PLC and Drive is Profibus
Thanks
The Transmission Media between PLC and Drive is Profibus
Thanks
Answers
Hi
From your question it is not so clear whether you are asking for help programming the drive or the PLC.
I can help you just for the drive: you can find attached an example of programming in Profibus, if that's what you needed.
Hope this help you
BR
Flavio
From your question it is not so clear whether you are asking for help programming the drive or the PLC.
I can help you just for the drive: you can find attached an example of programming in Profibus, if that's what you needed.
Hope this help you
BR
Flavio
Add new comment