Freelance 2019 Emulator incompatible DMS version
Hello,
I am using Freelance Engineering 2019 and tried to simulate the program without physical hardware.
For this, i followed the given steps of the tutorial, initializing a controller via localhost:8888 and the ip adress 127.0.0.1
When i try to load the software the error 'incompatible DMS version' pops up.
The Help file for this error reads 'The firmware or operating system version of the controller does not correspond the Freelance software'.
Since I am using the Emulator, how can I choose/update its firmware version compatible with Freelance 2019?
Is there a different solution?
Thanks in advance,
Answers
Hello
Please check about the custom functions that you have installed during freelance 2019 software installation.
Please uncheck the DMS related functions in custom tab.
Please check about the custom functions that you have installed during freelance 2019 software installation.
Please uncheck the DMS related functions in custom tab.
Add new comment