AfwCSLib error in IMS2 server- event viewer
During the check of event viewer on IMS2 server they found following error:
AfwCSLib Message Queue Full (see attached picture)
This error appears every day at the same time.
can anyone please help with explanation what does it mean and how to fix it?
Thank you in advance!
Voted best answer
Based on the frequency, early hours and hsHistoryService process name, likely a problem with the automated daily database consistency check.
I suggest running a "hsdbmaint -checkDB" interactively in an elevated command shell.
Errors (>0 values among the numerous check items) should be investigated and corrected (hsdbmaint -clean) until the check passes w/o errors.
"hsdbmaint" is documented in the IM Configuration Users Guide.
It is also recommended to run a consistency check on all Log Template and Log Configuration aspects. Use Plant Explorer's Find Tool to search for aspects of the two mentioned aspect categories (filter for Aspect Category = ...), drag & drop the search result to the Consistency Checker tool. Scan. Fix or delete.
Add new comment