How to use two acs880 drive module as single drive
I have considered two ACS880 Drive, rating of 585A (ACS880-04-585A-3+P944) and i want to use as single drive. Can any one suggest me, what are the accessories required? If any document available, kindly share.
Answers
Hi
I don't believe, to my knowledge, that you can turn two drives built to work independently, into a single single drive, i.e. effectively parallel the two drives. To do this action it is necessary that both the power of the drives and the drive control are specially designed and built. If you need a drive with a total power equal to or greater than the values you declared, I suggest you contact the closest ABB dealer or service that will be able to advise you best for your application.
BR
Flavio
I don't believe, to my knowledge, that you can turn two drives built to work independently, into a single single drive, i.e. effectively parallel the two drives. To do this action it is necessary that both the power of the drives and the drive control are specially designed and built. If you need a drive with a total power equal to or greater than the values you declared, I suggest you contact the closest ABB dealer or service that will be able to advise you best for your application.
BR
Flavio
Add new comment