2 questions reguarding the PM5630 visualization
Hello
I have imported a background image and I'm just wondering if there is a way of changing the size of the image within Automation Builder?
The background is being used in a visualization in Automation Builder 2.2
The PLC is PM5630
I feel like this second question might be a stupid question but I have spent some time on it and it has me stumped at this point.
I just want to rotate an object. I don't want it animated just need it rotated statically.
I found the section in the Help about this and it says that there should be a little handle above my object but I don't have that little handle. I also do not have a rotation option in the properties of my object. I have attached pictures of the Help menu, my object and the object properties.



Thanks for your Consideration!
I have imported a background image and I'm just wondering if there is a way of changing the size of the image within Automation Builder?
The background is being used in a visualization in Automation Builder 2.2
The PLC is PM5630
I feel like this second question might be a stupid question but I have spent some time on it and it has me stumped at this point.
I just want to rotate an object. I don't want it animated just need it rotated statically.
I found the section in the Help about this and it says that there should be a little handle above my object but I don't have that little handle. I also do not have a rotation option in the properties of my object. I have attached pictures of the Help menu, my object and the object properties.



Thanks for your Consideration!
Answers
This question has not yet been answered.
Add new comment