ACS850-04 demo suitcase replace with ACS880-01
Hello everybody.
I have not much experience with ABB ACS850-04 and ACS880-01. I have problem to operate ACS880-01 drive on ACS850-04 demo suitcase.
I replaced ACS850-04 inverter drive replaced by ACS880-01 drive and connect 3GVA052002-ASA motor.
The parameter setting was done and external command (DI) was set. But it did not work and no fault or error.
I also tried drive composer software to run the motor. It did not work too even communication was succesful.
I have attached some pictures about the drive in this post.
Are there anyone who help with this issue.
Thank you so much for your support.
Baagii
Answers
Hi,
Look the symbol on control panel:
![]()
![]()
The source of the inhibiting signal that is preventing the drive from starting you can find in 06.18
For details, read the corresponding manuals (3AUA0000085967, 3AUA0000085685) Source: 3AUA0000085967, 3AUA0000085685
Look the symbol on control panel:
The source of the inhibiting signal that is preventing the drive from starting you can find in 06.18
For details, read the corresponding manuals (3AUA0000085967, 3AUA0000085685) Source: 3AUA0000085967, 3AUA0000085685
by kstoilov
https://forum-controlsystems.abb.com/20242735/ACS880-1-has-some-problem
Add new comment