Compact Control Builder Project open issue.
When i want to open an project via compact control builder then some error is coming which is in the attachment.
Answers
Hi,
This error is showing that one of your library is missing from the folder path shown.
When did you get this error? Someone must have deleted the library or maybe moved it to some other location.
This error is showing that one of your library is missing from the folder path shown.
When did you get this error? Someone must have deleted the library or maybe moved it to some other location.
Did you take the backup in compact builder format ?
Do you have multiple project in your laptop ?
Your compact version is matching with the backup taken ?
Do you have multiple project in your laptop ?
Your compact version is matching with the backup taken ?
Refer to the same library in existing program and copy paste it in Hwlibraries of Program x86 .This issue will be resolved.
Add new comment