Data refresh in integration between two System 800xA using OPC client connection
Hello,
We have two System 800xA, one in version 6.0.3.3 and other one in version 5.1 Fp4 rev D. Between those Systems we have an OPC client connection configuration and PLC connect to send and receive the date in both ways.
When we send information from the plant that has System 800xA version 6.0.3.3 to the System 800xA with version 5.1, some variables doesn't refresh or displays an incorrect value (the first image represents the information read from the OPC client of the system 6.0.3.3 in the System 5.1. The image on the right is the motor that is operating).

The addressing seems to be OK, because we can browse through the data in the System 800xA server and connect the variable. The deploy function works without any issues.
Best regards,
We have two System 800xA, one in version 6.0.3.3 and other one in version 5.1 Fp4 rev D. Between those Systems we have an OPC client connection configuration and PLC connect to send and receive the date in both ways.
When we send information from the plant that has System 800xA version 6.0.3.3 to the System 800xA with version 5.1, some variables doesn't refresh or displays an incorrect value (the first image represents the information read from the OPC client of the system 6.0.3.3 in the System 5.1. The image on the right is the motor that is operating).


The addressing seems to be OK, because we can browse through the data in the System 800xA server and connect the variable. The deploy function works without any issues.
Best regards,
Answers
This question has not yet been answered.
Add new comment