Opening HGS Base Project (.ebp) in S+E V2.2
Hi,
I'm creating new Project with HPC using HGS , and after i read HGS manual I've found that there is an existing base project that i can use and modify to speed up the CLD configurations.
Now, I'm having troubles opening the existing project in S+E (HGS Base project).
i can't file where i can import the project in my Project admin list and it's not mentioned in the control engineering user manual
I'm creating new Project with HPC using HGS , and after i read HGS manual I've found that there is an existing base project that i can use and modify to speed up the CLD configurations.
Now, I'm having troubles opening the existing project in S+E (HGS Base project).
i can't file where i can import the project in my Project admin list and it's not mentioned in the control engineering user manual
Voted best answer
Hi,
The HGS 7.1 base and example projects are located in folders in the HGS program folder. The projects are Composer 6.0.1 version and so opening them in S+E 2.2 will require that they are upgraded. Firstly, extract the base project files from the .zip file to a temporary location. In S+E 2.2 follow the upgrade dialog from the project administration screen and you will see "Select any old project to upgrade" and a button with "...". Click the button and use the file open dialog to navigate to where the project was unzipped to and select the .ebp file. The base project should then appear in the S+E 2.2 project administration window. If the upgrade dialog is not available in S+E you may either be trying to do the upgrade from a client rather than the server or you don't have the required role as defined by S+E 2.2 user management.
BR,
Alan
The HGS 7.1 base and example projects are located in folders in the HGS program folder. The projects are Composer 6.0.1 version and so opening them in S+E 2.2 will require that they are upgraded. Firstly, extract the base project files from the .zip file to a temporary location. In S+E 2.2 follow the upgrade dialog from the project administration screen and you will see "Select any old project to upgrade" and a button with "...". Click the button and use the file open dialog to navigate to where the project was unzipped to and select the .ebp file. The base project should then appear in the S+E 2.2 project administration window. If the upgrade dialog is not available in S+E you may either be trying to do the upgrade from a client rather than the server or you don't have the required role as defined by S+E 2.2 user management.
BR,
Alan
Add new comment