Control Builder Safe
I have following question regarding Control Builder safe,
1. Is it possible to edit PG2 Graphic display?
2. Can we use panel 800 with AC800M Hi controller using Control builder safe?
3. If yes then is it possible to write variable from panel800 to AC800M Controller?
Thanks and regards,
1. Is it possible to edit PG2 Graphic display?
2. Can we use panel 800 with AC800M Hi controller using Control builder safe?
3. If yes then is it possible to write variable from panel800 to AC800M Controller?
Thanks and regards,
Answers
This question has not yet been answered.
by Mr Control Rank: 633 on 12/20/2020 11:01:18 PM | Like (1) | Report
1. Yes.
2. Yes, use MMS variables.
3. Yes, but the panel is NOT SIL classed. You cannot change SIL variables from the panel, technically it's possible, but it's not allowed according to rules and regulations.
Add new comment