Advant AC450 DataSet set ACT=0 will keep the data at REFs (DATs)??
I have to add more DAT(R) to the REF of a DS Element.
To connect more REFs the DS has to be set to ACT=0.
Unfortunately its on a running site. It is no problem if the existing data will be frozen but it should not reset, means set all REFs to "0".
I think the the DATs will keep the current value when setting ACT=0 but maybe someone can confirm 100%.
Thanks a lot
Andy
To connect more REFs the DS has to be set to ACT=0.
Unfortunately its on a running site. It is no problem if the existing data will be frozen but it should not reset, means set all REFs to "0".
I think the the DATs will keep the current value when setting ACT=0 but maybe someone can confirm 100%.
Thanks a lot
Andy
Answers
This question has not yet been answered.
by Jan.Sommer Rank: 1855 on 12/22/2020 6:06:23 AM | Like (0) | Report
Do I need to keep BLOCKED = 1 to keep the current values for additional new DATs to the DS?
Add new comment