AC500 eCo/standard , LD GBR-01
Hi
1-Can AC500-eCo I/O modules be used for AC500 standard(PM573 for me)?
2- How can I take the encoder pulses from the CPU(AC500) as output and give it to an encoder interface(LD GRB-01)?
Thanks.
1-Can AC500-eCo I/O modules be used for AC500 standard(PM573 for me)?
2- How can I take the encoder pulses from the CPU(AC500) as output and give it to an encoder interface(LD GRB-01)?
Thanks.
Voted best answer
Hi
1- Yes, AC500-eCo series I / O modules can be used on PM573-583-590 CPUs etc. and vice versa, you can check it directly during a configuration on Automation Builder.
2- this question is not very clear: maybe you want to use the pulses of an encoder read by the CPU (for example using the fast counter channels -> see the channel configuration in Automation Builder) to drive another device?
What do you mean by LD GRB-01?
If you give us more information, we can help you better
BR
Flavio
1- Yes, AC500-eCo series I / O modules can be used on PM573-583-590 CPUs etc. and vice versa, you can check it directly during a configuration on Automation Builder.
2- this question is not very clear: maybe you want to use the pulses of an encoder read by the CPU (for example using the fast counter channels -> see the channel configuration in Automation Builder) to drive another device?
What do you mean by LD GRB-01?
If you give us more information, we can help you better
BR
Flavio
Add new comment