CP635 with 2 protocols
Using a CP635 (B0) with 2 protocols, S7ETH and Ethernet/IP but there is no communication on the 2 selected protocols.
I have made a small project with 2 tags one from Siemens PLC, and one from Allen Bradley PLC.
It's programmed in Panel Builder 600 ver. 2.6.1 Build 175, Downloaded protocol for Siemens "PB610-V2.6-S/ET159 for Siemens, and PB610-V2.6-ETIP161 for the Ethernet/IP. The Panel Builder is running on trail license.
Starting the "Run/simulation" in the Panel Builder, and don't use the "use simulation" mode - then the values from the 2 PLC's is read correctly - but in the CP635 is not read, there is a blue question, and the value is not updated.
I Wireshark I can't see any request from the panel to the 2 PLC's
What do I miss ??
I have made a small project with 2 tags one from Siemens PLC, and one from Allen Bradley PLC.
It's programmed in Panel Builder 600 ver. 2.6.1 Build 175, Downloaded protocol for Siemens "PB610-V2.6-S/ET159 for Siemens, and PB610-V2.6-ETIP161 for the Ethernet/IP. The Panel Builder is running on trail license.
Starting the "Run/simulation" in the Panel Builder, and don't use the "use simulation" mode - then the values from the 2 PLC's is read correctly - but in the CP635 is not read, there is a blue question, and the value is not updated.
I Wireshark I can't see any request from the panel to the 2 PLC's
What do I miss ??
Answers
This question has not yet been answered.
Add new comment