Is it possible to use DP840 with AC450?
I suppose no, so the only way to replace DSDP150 is to use 6 x DP820?
Voted best answer
Hello.
DP840 is not supported in AC450 on AF100.
DP820 is OK with AC450.
It might be possible to configure and use DP840 on Profibus using Profibus Ci541 in Ac450 and a Profibus CI801or CI840 slave.
Anyhow, The parameterisation of Profibus devices in AC400 is rudimentary and do require deep understanding in the Profibus concept.
I have not heard anyone who have tried to use DP840 on Profibus together with AC450 but we have several customers who are using
standard S800 AI, AO, DI & DO boards on a CI801 or CI840 Profibus slave together with AC 450
BR
Jan-Erik
Add new comment