PM 573 ETH CM 574 RS Module Error
Hi All,
I have 1 PM 573- ETH R0271 CPU and two CM 574 RS communication modules. I add modules in the Automation Builder and i can't run PLC because these modules gives error. After i clear the error message in the PLC, PLC is running but i can't run these modules and these modules gives error continuously.
Are the firmware versions of PLC and modules suitable? Error messages and firmware versions in the attached picture.Please see attached picture.
Can anyone face similar kind of issues before, give me a suggestion?
I have 1 PM 573- ETH R0271 CPU and two CM 574 RS communication modules. I add modules in the Automation Builder and i can't run PLC because these modules gives error. After i clear the error message in the PLC, PLC is running but i can't run these modules and these modules gives error continuously.
Are the firmware versions of PLC and modules suitable? Error messages and firmware versions in the attached picture.Please see attached picture.
Can anyone face similar kind of issues before, give me a suggestion?
Answers
This question has not yet been answered.
by kstoilov
Hi.
Look at ABB site
https://new.abb.com/plc/programmable-logic-controllers-plcs/ac500/communication-modules
under information tab there is a document for firmware versions etc. Most probably you need to adjust/downgrade some firmware (info from your picture No.2)
Add new comment