Zenon reporting & automatically turns off without any pop-up message
Dear sir,
We have the following configuration:
PLC Hardware -PM590 v1 CPU
PLC Software - Codesys 2.3
SCADA Software- Zenon 7.60 64bit (Operator version)
OS- Windows 7-64bit
Protocol-OPC Client V2-0
Currently, we are facing some problems like
1. SCADA system automatically turns off without any pop-up message.
2. After reopening Zenon run time, old Trends graphs are vanishing from the trend.
Earlier we had problems with pop-up messages on the SCADA Screen (picture attached).
if we tried to remove it from any of three SCADA's (SERVER-1 & CLIENT-2) than the Computers getting stop.
sir, please guide me for the permanent solution.
Answers
Hello Sanjeev,
If you are using ABB zenon 7.60 version then you can contact local ABB Support executive to help you on this topic.
Could you please let me know below details to forward your request to the local team:
1. Company name
2. Address
If you are using ABB zenon 7.60 version then you can contact local ABB Support executive to help you on this topic.
Could you please let me know below details to forward your request to the local team:
1. Company name
2. Address
Add new comment