SPlus Operation & HW Diagnostic Tags
Dear i wanted to make Diagnostic Tags that provides information me on the Server & On Display Builder that
1. The Ping is Lost from Controller, GPS Clock or any Server, Operator or Engineering PC.
2. S+ Operation Application is Closed from the particular System.
I have the Default Tags that are created in TagData base of Operation Engineering.
Thanks
1. The Ping is Lost from Controller, GPS Clock or any Server, Operator or Engineering PC.
2. S+ Operation Application is Closed from the particular System.
I have the Default Tags that are created in TagData base of Operation Engineering.
Thanks
Answers
See attached database export for DEVSTAT tag for an operator client. I think this will answer your first point. Just make sure the node is present in the host files in the system.
Regards
Are
Regards
Are
Add new comment