Download project to soft controller 5.1
Hi,
I am trying to download my project for soft controller, but during that I have got error(no connection), please advise me what I should do?
please see attended picture
I am trying to download my project for soft controller, but during that I have got error(no connection), please advise me what I should do?
please see attended picture
Voted best answer
Is soft controller running? Have you configured it for that IP address / port?
Answers
You will need to fix your connectivity to the IP address shown. As you did not mention what version you are using, you may need to put a switch on your NIC to 'enable' the port or use the loopback address of 127.0.0.1:2
First you need to simulate hardware.
Allow HWSimulation:
![]()

Then right click hardware and select simulate hardware.
System identity should be 127.0.0.1:2 if your softcontroller is running on the same machine.
Ethernet port 1 should have 127.0.0.1
Allow HWSimulation:
Then right click hardware and select simulate hardware.
System identity should be 127.0.0.1:2 if your softcontroller is running on the same machine.
Ethernet port 1 should have 127.0.0.1
Add new comment