I want to know PM583-ETH and ACS380 communication
Voted best answer
Hi
maybe if you explained better what you want to do, you could get some precise answers.
If you want to connect an ACS380 drive to a PM583-ETH cpu, you can use for example the modbus on the com port of the cpu and the modbus connection card on the drive; or you can use an interface of your choice from all of the following types: profinet profibus ethercat .....
ethernet IP
....
you can read all the available protocol types in the product catalog on the CPU you will have to mount the communication master for each type of protocol and on the drive the corresponding communication slave module. If you don't explain better what you want, we can't help you better ....
BR
Flavio
maybe if you explained better what you want to do, you could get some precise answers.
If you want to connect an ACS380 drive to a PM583-ETH cpu, you can use for example the modbus on the com port of the cpu and the modbus connection card on the drive; or you can use an interface of your choice from all of the following types: profinet profibus ethercat .....
ethernet IP
....
you can read all the available protocol types in the product catalog on the CPU you will have to mount the communication master for each type of protocol and on the drive the corresponding communication slave module. If you don't explain better what you want, we can't help you better ....
BR
Flavio
Answers
In the Automation Builder you will find under
Help > Project examples
a Link to the autoamatically installed examples and additional libraries of AC500
C:\Users\Public\Documents\AutomationBuilder\Examples
There check out the folder
PS553-DRIVES
You find explanation and examples to connect AC500 to ACSxxx drives via Profibus, Profinet, Modbus RTU, Modbus TCP,..
Help > Project examples
a Link to the autoamatically installed examples and additional libraries of AC500
C:\Users\Public\Documents\AutomationBuilder\Examples
There check out the folder
PS553-DRIVES
You find explanation and examples to connect AC500 to ACSxxx drives via Profibus, Profinet, Modbus RTU, Modbus TCP,..
Source: C:\Users\Public\Documents\AutomationBuilder\Examples
Add new comment