FENA-11 Modbus TCP adapter
Dear All
I have a PV980 Central inverter with FENA-11 Ethernet Modbus TCP protocol adapter, the problem is the FENA-11 maximum can accept 2 client connection at one time, and the two clients are used from two Modbus master devices, please advise if there a method to make the FENA module accept more then two connection for example, accept three connections at the same time two.
I have a PV980 Central inverter with FENA-11 Ethernet Modbus TCP protocol adapter, the problem is the FENA-11 maximum can accept 2 client connection at one time, and the two clients are used from two Modbus master devices, please advise if there a method to make the FENA module accept more then two connection for example, accept three connections at the same time two.
Answers
This question has not yet been answered.
Add new comment