800xA 5.1 RevD Rollup System Update Tool
Hi,
I'm relatively new in 800xA and this is my first installation/update.
I need to update 800xA 5.1 RevD so I can have Control Builder Version 5.1.0-3 (Build 5.1.1300.10) (right now is Version 5.1.1-1 (Build 5.1.1110.3)).
Instructions I've got are:
800xA System Update Tool User Instruction (2PAA106938-510C)
System 800xa 5.1 RevF Release Notes New Functions and Known Problems (2PAA111287-510)
They are not too useful for installation process.
In installation media (picture) there is "Autorun.exe" but it installs products like: 3rd party, SoftPoint Server, PLC connect etc. there is no Control builder update.
Can someone explain me what is installation procedure?
Answers
Hello
Software 800xA 5.1 has two software alternatives, the original and Feature Pack.
In Programs and Features you can see whether 800xA Base contains FP (Feature Pack) or not.
I assume you have FP4 as Build 5.1.1110.3 is included in 5.1 FP4 RevD.
Don't upgrade just a specific software, like CBM, upgrade the whole 800xA 5.1.
Let's say you have 800xA 5.1 FP4 RevD today,
then upgrade to 5.1 FP4 Rev E. (RevE needs IE11 for W10 and WS 2016 64 Bit)
If you don't have FP you go to System Update Tool folder and execute the executable.
and if you have FP then you go to System Feature Pack Update Tool folder.
/Ronny
Software 800xA 5.1 has two software alternatives, the original and Feature Pack.
In Programs and Features you can see whether 800xA Base contains FP (Feature Pack) or not.
I assume you have FP4 as Build 5.1.1110.3 is included in 5.1 FP4 RevD.
Don't upgrade just a specific software, like CBM, upgrade the whole 800xA 5.1.
Let's say you have 800xA 5.1 FP4 RevD today,
then upgrade to 5.1 FP4 Rev E. (RevE needs IE11 for W10 and WS 2016 64 Bit)
If you don't have FP you go to System Update Tool folder and execute the executable.
and if you have FP then you go to System Feature Pack Update Tool folder.
/Ronny
by ParthibanT Rank: 42 on 10/20/2020 1:39:30 AM | Like (2) | Report
From which version to which version you want to update? Any typo in the question version details?
Add new comment