VP800 Turbine module Coil capacity
Thanks in advance.
According to the manual, the VPM810 output is voltage calculated from Coil Resistance setting and Max/Min coil current(When Close loop mode Min is minus Max).
If I want to control a actuator type -10V/+10V no matter what the coil resistance really is, can I simply set the coil resistance to 1k and Max coil current to 10mA? And there must be some limitation as the power is only 24VDC. What is the limitation? As we know, the output limit is -200mA to 200mA. However, according to the manual there is no Max Coil Resistance setting limit.
If the real coil is 10k, can I set the Coil Resistance to 10k and Max coil current to 1mA?
According to the manual, the VPM810 output is voltage calculated from Coil Resistance setting and Max/Min coil current(When Close loop mode Min is minus Max).
If I want to control a actuator type -10V/+10V no matter what the coil resistance really is, can I simply set the coil resistance to 1k and Max coil current to 10mA? And there must be some limitation as the power is only 24VDC. What is the limitation? As we know, the output limit is -200mA to 200mA. However, according to the manual there is no Max Coil Resistance setting limit.
If the real coil is 10k, can I set the Coil Resistance to 10k and Max coil current to 1mA?
Answers
This question has not yet been answered.
Add new comment