one digit of physically digital output not working well
Good morning
Dire sir
I am using freelance 2013 ACS900F and I have a problem with one of the logic output points when I give drive command the signal in the physical output point is blinking and not continuous even though all the conditions in the FB (Individual drive function) are all correct. PR0 = 0 IN = 1 LOC = 0 AND AFTER THE FEEDBACK COME THE FB1 = 1 FB0 = 0 FLT = 0 OUT = 1 (CONTINUOUSLY) BUT OUTPUT in the physically digital output IS BLINKING I have changed the logical output point to another card and also changed the Individual drive function (IDF), but the result is same not changed. Can you explain this strange phenomenon to me, please?
Thank you so much
Best regards
Answers
This question has not yet been answered.
by Dieter Henkel
What I/O module are you using?
by almohayak Rank: 575 on 10/16/2020 12:15:12 AM | Like (0) | Report
Hello Mr. Dieter Henkel
thank you for your answer, and I want t to inform you the digital output is DO818.
Best regards
Add new comment