CHMI Locked
Dear sir,
Kindly check the given attachment and it shows a locked symbol for the system
What does this mean? How it occurs and what are my options now pls advice
wr
Kindly check the given attachment and it shows a locked symbol for the system
What does this mean? How it occurs and what are my options now pls advice
wr
Voted best answer
No need to salute on this forum... :-)
The lock icon is set when the 800xA Service Account that was configured during installation of System 800xA has failed to logon a service, etc.
Verify that the service account password is correctly configured, then re-run System Software User Settings using the classic Configuration Wizard.
The lock icon is set when the 800xA Service Account that was configured during installation of System 800xA has failed to logon a service, etc.
Verify that the service account password is correctly configured, then re-run System Software User Settings using the classic Configuration Wizard.
Add new comment