Configuration of AC500 with CI521
Hello,
I have a PM-573-ETH with AI523 and CI521, the CI521 would be connected to the AI523 and using Ethernet all inputs will be available to PM573-ETH.
Is there a clear guide to configure CI521 to be able to read the inputs from the PLC?
Thanks,
Osama Ayoub
I have a PM-573-ETH with AI523 and CI521, the CI521 would be connected to the AI523 and using Ethernet all inputs will be available to PM573-ETH.
Is there a clear guide to configure CI521 to be able to read the inputs from the PLC?
Thanks,
Osama Ayoub
Answers
Dear Osama,
The attached document has a guide for CI521-MODTCP configuration. I do hope to be useful for you.
Regards.
The attached document has a guide for CI521-MODTCP configuration. I do hope to be useful for you.
Regards.
Add new comment