How to install secondary server in 800xA ver 6.1(Redundant Controller)
Hello Everyone
I have installed primary server and for installation of secondary server whether i have to follow the same configuration which i have done for primary server or else any other changes in configuration. Pls help me in installation. As mentioned above we are using a redundant network
Thanks in advance
I have installed primary server and for installation of secondary server whether i have to follow the same configuration which i have done for primary server or else any other changes in configuration. Pls help me in installation. As mentioned above we are using a redundant network
Thanks in advance
Voted best answer
Hi
Please make sure you have run the NPT tool in secondary server, before deploy the node functions in secondary server. NPT will copy the media to the local repository and install the 800xA Base and CLS.
Once NPT successfully completed. Allocate system functions to both Primary & secondary server then, click 'Make Redundant' in node configuration tab in System Configuration Console(SCC) which make secondary as redundant to primary server. Then finally give 'Deploy'
Answers
Pls check below thread which talks about similar requirement,
https://forum-controlsystems.abb.com/...
Are you using IEC Connect? If yes, then special attention required for IEC connect v6.1 installations. For details, refer installation manual.
https://forum-controlsystems.abb.com/...
Are you using IEC Connect? If yes, then special attention required for IEC connect v6.1 installations. For details, refer installation manual.
Add new comment