Advacommand 1.9/0 -Advabuild 2.9/1 For Mod300 / Failed to install Environment
Hi , could you support in the following issue ?
We have installed an OS/ES installed and we are installing and OS we have installed advacommand software and after doing that when it reached the advacommand interface windows we disconnected the eDCN cables and set as standalone node S , It booted properly and we could download ADVANT environment.
After that we restarted again the OS and we set the dcn addres according to database configuration, we waited until the OS booted completely it showed FROM which it should show the hostname but it showed NONE and it showed it showed "could not find the server node" then and we tried to download the ADVANT Environment it shows that ADVANT environment was not found . Despite of when we booted the node as Standalone it had ADVANT Environment into.
OSES looks fine and the advabuild database is fine , we can see OS node from system status active and running
Also the time from OS after booting is 01 JAN 1970 , it looks like RTAB from OSES is not broadcasting the time eventhough its time from OSES is according to the date and time of the country.
We have tried to boot others 2 OS station and they have had the same behavior as I have mentioned above
Also When we try to open the environment builder at Advacommand Startup Interface , it shows the following
Try to connect to Oracle went to error
The sqlcode : -1034
Error during execution
ORA-00134 Oracle not available
ORA-0738: swget open error
Thanks for your support
Regards
Ricardo
We have installed an OS/ES installed and we are installing and OS we have installed advacommand software and after doing that when it reached the advacommand interface windows we disconnected the eDCN cables and set as standalone node S , It booted properly and we could download ADVANT environment.
After that we restarted again the OS and we set the dcn addres according to database configuration, we waited until the OS booted completely it showed FROM which it should show the hostname but it showed NONE and it showed it showed "could not find the server node" then and we tried to download the ADVANT Environment it shows that ADVANT environment was not found . Despite of when we booted the node as Standalone it had ADVANT Environment into.
OSES looks fine and the advabuild database is fine , we can see OS node from system status active and running
Also the time from OS after booting is 01 JAN 1970 , it looks like RTAB from OSES is not broadcasting the time eventhough its time from OSES is according to the date and time of the country.
We have tried to boot others 2 OS station and they have had the same behavior as I have mentioned above
Also When we try to open the environment builder at Advacommand Startup Interface , it shows the following
Try to connect to Oracle went to error
The sqlcode : -1034
Error during execution
ORA-00134 Oracle not available
ORA-0738: swget open error
Thanks for your support
Regards
Ricardo
Answers
Hello,
this is an answer related to the time. Timesynch in the Unix World doesn't work anylonger since 2020-01-01. There is a bug in the timesynch code which is only fixed for AC460 and AdvaBuild 3.7.
So for Advant Unix you have to enable Reverse Time Synch and the use i.e. NTP to make sure they have the same time.
BR Stefan
this is an answer related to the time. Timesynch in the Unix World doesn't work anylonger since 2020-01-01. There is a bug in the timesynch code which is only fixed for AC460 and AdvaBuild 3.7.
So for Advant Unix you have to enable Reverse Time Synch and the use i.e. NTP to make sure they have the same time.
BR Stefan
by ricardo.marrero.a Rank: 158 on 9/11/2020 7:46:45 PM | Like (0) | Report
Also I have verified tnsnames.ora and listener.ora and I compared them against the OSES files only differences is hostname of course because they are different nodes with different hostnames
Regards
Ricardo
Add new comment