Issue in using Custom project based Logical Colors in 800xa?
I have defined customized Project based Logical Color aspect and added colors in Workplace Structure > Web System Workplace.
Now I linked colors with the object project Fill/Pen Color Property in PG2 Graphics and it is showing defined color
but issue is when I change the RGB color in Logical Color in Workplace Structure > Web System Workplace but it does not show changed color.
Now I linked colors with the object project Fill/Pen Color Property in PG2 Graphics and it is showing defined color
but issue is when I change the RGB color in Logical Color in Workplace Structure > Web System Workplace but it does not show changed color.
Answers
Is the color defined in more than one Logical Color aspect? It's possible it is being overwritten from a child/parent object.
Hi,
I understand that change in the Logic colour aspect is not reflecting, try to restart the workplace, i too had faced the same issue it is resolved after restarting the workplace.
I understand that change in the Logic colour aspect is not reflecting, try to restart the workplace, i too had faced the same issue it is resolved after restarting the workplace.
Add new comment