Acs550 and high speed motor wont work
Cant get my acs550 to work with high speed motor. I have looked over my setting. Getting fault code 1009. Motor spec: 2.2kw 220v 10a 400hz
Any advice?
Thanks.
Any advice?
Thanks.
Answers
Hi
to give you more advice, I suggest you post a photo of the motor nameplate and indicate the characteristics of your ACS550, you can put a photo of the drive nameplate.
Are you using the drive in V / F or vector mode? Did you do an ID run in case you are using it in vector?
Was the motor designed to achieve these speeds?
If you give us more information, we can help you better
BR
Flavio
to give you more advice, I suggest you post a photo of the motor nameplate and indicate the characteristics of your ACS550, you can put a photo of the drive nameplate.
Are you using the drive in V / F or vector mode? Did you do an ID run in case you are using it in vector?
Was the motor designed to achieve these speeds?
If you give us more information, we can help you better
BR
Flavio
by havard.langvik Rank: 5868 on 9/10/2020 4:40:48 PM | Like (0) | Report
And 24000rpm
Add new comment