can we configure redundant sntp for redundant controllers in 800xA
Answers
A redundant AC 800M controller consists of a primary (running) controller and a backup (not running) controller with hot/instant failover capability.
The running controller can be set to slave to two (2) SNTP sources (the controller will choose which one to use).
The CBM > Clock Synchronization tool and controller log will detail the status.
The running controller can be set to slave to two (2) SNTP sources (the controller will choose which one to use).
The CBM > Clock Synchronization tool and controller log will detail the status.
Add new comment