problem with importing database
I have problem with importing tag
the error is "0474B-VE217 is INFI/HARMONY type , not allowed to importOnly RCM / DIGITAL / N90STA tagtypes are allowed"
HINT: the tag type is MSDD
the error is "0474B-VE217 is INFI/HARMONY type , not allowed to importOnly RCM / DIGITAL / N90STA tagtypes are allowed"
HINT: the tag type is MSDD
Voted best answer
Hi,
The version information is missing but the below information remains same across S+ Engineering 2.x versions.
The INFI tags are not allowed to import from Operations Engineering (Composer Operations). Only the N90STA is allowed to import for diagnostic purpose. This is the design from S+ Engineering 2.x onwards. Perform "Synchronize Tags" from ribbon bar and all the Harmony tags gets created in Operations engineering (Composer Operations). Refer to user manual for more information.
Note:
Name change from Composer Operations to Operations Engineering is from S+ Engineering 2.x versions.
For exact S+ engineering version information, please refer to release notes.
Regards,
Farooq
The version information is missing but the below information remains same across S+ Engineering 2.x versions.
The INFI tags are not allowed to import from Operations Engineering (Composer Operations). Only the N90STA is allowed to import for diagnostic purpose. This is the design from S+ Engineering 2.x onwards. Perform "Synchronize Tags" from ribbon bar and all the Harmony tags gets created in Operations engineering (Composer Operations). Refer to user manual for more information.
Note:
Name change from Composer Operations to Operations Engineering is from S+ Engineering 2.x versions.
For exact S+ engineering version information, please refer to release notes.
Regards,
Farooq
Add new comment