800xA Client installation error

During Deploying from server to client i am getting this error posted here....
Please suggest what could be the cause.
i am using 800xA 6.1.0 with server 2016 OS
Client side : WINDOWS 10 ENT 2016 LTSB
Answers
Hello,
Check all pre-requisite met like HW/OS compatibility, required W patches, 3rd party sw, etc...
Based on image seems like client node not able to connect to Pri AS/CS, looks like network issue...
Check that all the nodes network cards set as per manual,
found on open Internet manual for network, https://library.e.abb.com/public/9c8b6c0dc8bdfe16c1257b400026feb3/3BSE034463-51
0_E_en_System_800xA_5.1_Network_Configuration.pdf, Page 132 onwards...
setting up network properly should resolve issue...
Else In ABB Lib look for getting started manual 2PAA111708-610, should help
Hope that helps....
Check all pre-requisite met like HW/OS compatibility, required W patches, 3rd party sw, etc...
Based on image seems like client node not able to connect to Pri AS/CS, looks like network issue...
Check that all the nodes network cards set as per manual,
found on open Internet manual for network, https://library.e.abb.com/public/9c8b6c0dc8bdfe16c1257b400026feb3/3BSE034463-51
0_E_en_System_800xA_5.1_Network_Configuration.pdf, Page 132 onwards...
setting up network properly should resolve issue...
Else In ABB Lib look for getting started manual 2PAA111708-610, should help
Hope that helps....
When using Windows Workgroup it is utmost important that all user accounts and user groups are synchronized across all computers.
A wrong password or group membership may explain why the client cannot connect to the server. RNRP must also be enabled and operational (server need to see the client)
A wrong password or group membership may explain why the client cannot connect to the server. RNRP must also be enabled and operational (server need to see the client)
Add new comment