Ladder diagram in control builder
Hello,
Is there a way to write ladder logic and insert rungs without an output coil?
For example I need to have a contact the is connected to the enable of a function block but without a coil at the end.
Thanks,
Osama Ayoub
Is there a way to write ladder logic and insert rungs without an output coil?
For example I need to have a contact the is connected to the enable of a function block but without a coil at the end.
Thanks,
Osama Ayoub
Answers
This question has not yet been answered.
by Amal Rank: 84 on 8/23/2020 9:24:22 PM | Like (0) | Report
Hi,
I am not used Control Builder I use Automation Builder and in here it is possible to make rungs as per your example
Add new comment