Hi, Is there a setting to limit the number of face plates that each operator can open in 800xA?
Answers
It can be configured in the View Class Reference aspect of Faceplate views in the library structure.By default,it is 0 (No limits)
https://forum-controlsystems.abb.com/1053115/Max-number-of-faceplates
https://forum-controlsystems.abb.com/1053115/Max-number-of-faceplates
Add new comment