Does Acs355 now build in modbus RTU as the catalogue mention got rs232 modbus RTU
Curious than Acs355 consider build in modbus RTU function or just connector need to add on option card to make this features
Answers
Hi
ACS355 can be used with ModBus 485 RTU using an FMBA-01 interface. It is a very cheap interface, generally used for applications where the transmission speed is not important and for a modest number of slave nodes.
In the manual it is indicated that communications can also be made using the RS232 connector of the panel, but I have never personally had the opportunity to deepen this type of use.
BR
Flavio
ACS355 can be used with ModBus 485 RTU using an FMBA-01 interface. It is a very cheap interface, generally used for applications where the transmission speed is not important and for a modest number of slave nodes.
In the manual it is indicated that communications can also be made using the RS232 connector of the panel, but I have never personally had the opportunity to deepen this type of use.
BR
Flavio
Add new comment