Input field interaction and bool dew is not taking any values
I want to give possibility of entering a real value from the display to operator. For that i am using Input field and configured all the parameters correctly in 800xA Rev 6.1.0.1. But I am not able to enter any value in it after saving. Same thing is happening with bool dew. I have checked doing same configuration in 800xA 6.0 version. there it is working fine. Any special configuration need to be done in 6.1.0.1 version to accept values from display?
Add new comment