USING ABB SIMATIC library to control ACS800 from Siemens S7-300
I am trying to Control the drive using the SIMATIC blocks Library provided by ABB .
I am using PPO4 and DP-V1 GSD and have set up the drive s per the instructions in the manual
I have set the following Parameters as well
98.02 COMM. MODULE LINK FIELDBUS Activates fieldbus module 98.07 COMM PROFILE ABB DRIVES Communication profile ABB drives 51.02 NODE ADDRESS [PB NODE] PROFIBUS DP node address of the drive 51.21 DP MODE [DP MODE] 1 for DPV1, 0 for DPV0 51.27 FBA PAR REFRESH REFRESH Updates fieldbus settings (groups 51 to 55) 10.01 EXT 1 STRT/STP/DIR COMM.CW Fieldbus interface as source for start and stop 11.03 EXT REF1 SELECT COMM.REF Fieldbus interface as source for speed reference 16.04 FAULT RESET SEL COMM.CW Fieldbus interface as source for fault reset (11.05) EXT REF1 MAXIMUM [Scale max] Max speed/frequency scaling value (used in function block/visualization input SPEED_REF_MAX).
Because of some reason the drive will not start running - Please help
I am using PPO4 and DP-V1 GSD and have set up the drive s per the instructions in the manual

I have set the following Parameters as well
98.02 COMM. MODULE LINK FIELDBUS Activates fieldbus module 98.07 COMM PROFILE ABB DRIVES Communication profile ABB drives 51.02 NODE ADDRESS [PB NODE] PROFIBUS DP node address of the drive 51.21 DP MODE [DP MODE] 1 for DPV1, 0 for DPV0 51.27 FBA PAR REFRESH REFRESH Updates fieldbus settings (groups 51 to 55) 10.01 EXT 1 STRT/STP/DIR COMM.CW Fieldbus interface as source for start and stop 11.03 EXT REF1 SELECT COMM.REF Fieldbus interface as source for speed reference 16.04 FAULT RESET SEL COMM.CW Fieldbus interface as source for fault reset (11.05) EXT REF1 MAXIMUM [Scale max] Max speed/frequency scaling value (used in function block/visualization input SPEED_REF_MAX).
Because of some reason the drive will not start running - Please help
Answers
This question has not yet been answered.
Add new comment