Application download
Hello
We have error when downloading application to pm866
Error1454: the application has simulation mark but declared in a not simulation marked controller
You can see error screnshot in appendix
We have error when downloading application to pm866
Error1454: the application has simulation mark but declared in a not simulation marked controller
You can see error screnshot in appendix
Voted best answer
From the error message, i understand that only the application is marked as simulated but the controller is not simulated.
To download a hardware configuration to a simulated controller:
- In the hardware tree, select the controller to be simulated.
- Right-click the controller, select Properties and make sure that Simulate Hardware is checked in the menu. The controller and all hardware units belonging to the controller will automatically be marked with a red "S"
- Download the hardware configuration to be simulated to the simulation controller by selecting Tools > Download Project and Go Online.
Add new comment