BDM Error- 800xa Version 6.0.3.2
I can able to create instances through BDM for types which are created in the application level.
But not able to create Instances through BDM for the Object level Types in the 800xa Version 6.0.3.2.
Getting
Error Message as:
"Warning: aspect is part of an object type and cannot be re-created or updated!"
"Commit transaction failed"
Details:Insert failed.
Reason: E_AFW_AOM_OBJECT_NOT_FOUND(0x8abb090a) Object not found in the object manager.
Error Code:
S_AFW_AOM_ACCESS_DENIED,0x8abb4400
Please Suggest an idea to resolve this issue.
Thanks in Advance.
But not able to create Instances through BDM for the Object level Types in the 800xa Version 6.0.3.2.
Getting
Error Message as:
"Warning: aspect is part of an object type and cannot be re-created or updated!"
"Commit transaction failed"
Details:Insert failed.
Reason: E_AFW_AOM_OBJECT_NOT_FOUND(0x8abb090a) Object not found in the object manager.
Error Code:
S_AFW_AOM_ACCESS_DENIED,0x8abb4400
Please Suggest an idea to resolve this issue.
Thanks in Advance.
Answers
This question has not yet been answered.
by ParthibanT Rank: 42 on 8/8/2020 10:19:21 AM | Like (0) | Report
Which user account you are using?, pls try to use Service or Installer account. Also pls make sure that there are no reservation issue.
by jagadheesan.s@in.abb Rank: 506 on 8/16/2020 12:40:49 PM | Like (0) | Report
Tried in all accounts and no reservation.Still problem is not solved.
Add new comment