Possible effects of Using Microsoft's System Center Endpoint Protection on 800xA Version 6.1
ABB officially tested and qualified two Antivirus Software in 800xA 6.1 -
McAfee Endpoint Security and Symantec Endpoint Protection for Optimal performance with 800xA operation.
Regular testing is being carried out for these two AV Software - Virus definition files releases and documents are being released on weekdays - available in ABB Library. ( 9ARD170703-012 )
We would like to know the possible effects that Client might face in the Plant for not using the recommended AV Software.
Example : Issues faced in any plant earlier.
Voted best answer
Performance issues, files get locked when the scanner search trough them.
Network analysis can also affect performance.
Been there done that :)
Network analysis can also affect performance.
Been there done that :)
Add new comment