Problem with pfeil01 MAK
Hello.
I have got a little file named pfeil01, a graphic macro that's impossible to delete.
This small file makes the program to crash as soon as you try to check it, rename it or open it.
When you export a project with this file in it, it´s impossible to import the project again.
In the end of the import process program crash. Even if the program crash there is a .PRO file
created but everything under hardware has disappeared.
Freelance is 2018SP1.
Anybody that have the same experience?
Regards
Tore Wassén
I have got a little file named pfeil01, a graphic macro that's impossible to delete.
This small file makes the program to crash as soon as you try to check it, rename it or open it.
When you export a project with this file in it, it´s impossible to import the project again.
In the end of the import process program crash. Even if the program crash there is a .PRO file
created but everything under hardware has disappeared.
Freelance is 2018SP1.
Anybody that have the same experience?
Regards
Tore Wassén
Answers
Dear Tore,
Hope and wish all is well at your end.
Very strange, however have you tried to placing that graphic in the pool and try checking node by node plausibility check.
Or try to export only that graphic from the project and delete it, then perform the plausibility see if that works.
and exported graphic page you can import back into other fresh project and see if that works or allowed ?
byetheway from where did you got Freelance 2018 SP1 software, I have never seen such version got ever released !!!
If you can not figure out would you like to share project .csv format....
Wbr
-/Sumit
Hope and wish all is well at your end.
Very strange, however have you tried to placing that graphic in the pool and try checking node by node plausibility check.
Or try to export only that graphic from the project and delete it, then perform the plausibility see if that works.
and exported graphic page you can import back into other fresh project and see if that works or allowed ?
byetheway from where did you got Freelance 2018 SP1 software, I have never seen such version got ever released !!!
If you can not figure out would you like to share project .csv format....
Wbr
-/Sumit
by Reda Rank: 99 on 7/23/2020 10:39:26 AM | Like (0) | Report
Hi
I understand that you are not able to delete
This mean it is used in the project
So first you need to remove from the project
Can you send screenshots of this part
by ToreWassen Rank: 73 on 7/23/2020 12:27:14 PM | Like (0) | Report
Hi
don´t understand what you mean. When I try to delete I get the answer that I´m not allowed to delete a macro that is used.
But, the macro is not used. The pointer where it is supposed to be used is empty, sometime I have seen is a chinese sign insted.
regards
Tore
by tr Rank: 67 on 7/25/2020 5:47:49 AM | Like (0) | Report
Have a look at the file. It's amazing where such a PRT file comes around everywhere. There are also parts of my attachments in there (user management salutes) I think something went wrong with the coordinates. I can import the macro with a change on me, but then I can't access the macro object. If I select and delete everything, I get the error "Macro is empty" after the plausible error " What should the contents of the macro be?
Regards
T.R.
by ToreWassen Rank: 73 on 7/25/2020 1:50:16 PM | Like (0) | Report
Hi all,
I have now found a solution to my problem.
In the CSV-file saved before upgrade to 2019SP1 the file exists.
Immedietly after import to 2019SP I´m allowed to open the pfeil01.
I chose select all and then delete the objects. Now I save the pfeil01 and after this
I can delete the little bugger.
The project became corrupt when I installed a UFB with a file named pfeil01 within it.
Now I have to import this fixed CSV file and perform a new Load Whole Station again on 9 PS.
Probably I must by some cake to the staff but I guess ABB will pay for this.....
Best regards
Tore
by Dieter Henkel
You could send the faulty PRO file to me. I could try to find the makro and delete it. Then incremental load would only be needed.
by ToreWassen Rank: 73 on 8/3/2020 4:27:02 AM | Like (1) | Report
Hi Dieter,
thanks for engaging in our problem.
The customer is Freudenburg Household Products and I´m normally not allowed to ecport the project file. I´ll try to see if there could be an exeption in this case.
I have had some other problems with this verson also.
I communicate with Jiri via Lars Mårtensson but there are no relevant answers.
To summarize, to date we have three unexplained "phenomena".
1: the file pfeil01 that corrupted the project.
2: An undeleted item that "got in the way" and eventually forced us to LoadWholeStation.
3: Some kind of capacity problem that makes the Save Parameters function
does not work properly.
I have worked with Freelance (Digimatik) since 1994 and never seen anything like this. But, now the system has been OK for almost a week,
mybe it was something temporary.
Very Best
/tore
Add new comment