65k tags Zenon Scada - Hardware Specification Requirements
Hi,
What are the required Hardware specifications for Server, Operator station, Mobile workstation (Laptop) for Zenon Scada with 65k tags.
Where can I find the reference documents?
Thanks!
What are the required Hardware specifications for Server, Operator station, Mobile workstation (Laptop) for Zenon Scada with 65k tags.
Where can I find the reference documents?
Thanks!
Answers
Hi Rahul,
65k tags are not too bag and zenon should be able to handle that with a standard server Hardware (For Example: Dual Core i7, 1.7 GHz processor, 16GB RAM), but the zenon performance is highly dependent on how many variables are "advised" at the same time.
Every variable that is archived or currently shown on a screen or there is an Alarm configured for it and so on is advised. The value changes per second has a bigger impact on the zenon performance than the total amount of variables in the project. Example: a project with 65k tags but only 1000 value changes per second might have a better performance than a project with 10k tags but 10k value changes per second.
65k tags are not too bag and zenon should be able to handle that with a standard server Hardware (For Example: Dual Core i7, 1.7 GHz processor, 16GB RAM), but the zenon performance is highly dependent on how many variables are "advised" at the same time.
Every variable that is archived or currently shown on a screen or there is an Alarm configured for it and so on is advised. The value changes per second has a bigger impact on the zenon performance than the total amount of variables in the project. Example: a project with 65k tags but only 1000 value changes per second might have a better performance than a project with 10k tags but 10k value changes per second.
Add new comment