Mask a variable value for 5sec everytime when the value is enabled.
Hi All,
System: Freelance AC800F
I want to retain the initial value for 5 second for a variable and then fetch the actual value from the field, is there any block (which i can trigger with other variable) to mask the value for some time & then overwrite with actual ones?
For example like feedback variables... etc
Thanks in Advance..
Regards,
Sri
System: Freelance AC800F
I want to retain the initial value for 5 second for a variable and then fetch the actual value from the field, is there any block (which i can trigger with other variable) to mask the value for some time & then overwrite with actual ones?
For example like feedback variables... etc
Thanks in Advance..
Regards,
Sri
Answers
The easiest way would be to use a SEL block with TON block as a delay.
Depending on the application, a UDF (User Defined Function) would be advantageous.
Maybe even easier :) a 'move' with an enable flag
Add new comment