Power Lib 3.0.0 and Power Generation Lib 1.0.0 issue
Hi Experts,
I have issue on 800xA system v5.0 that Power Lib 3.0.0 and Power Generation Lib 1.0.0 in Function Block AIS and ais, has an issues when compile the existing project.
Both library is protected so no change / modification on both library.
But the issue pop up on existing logic like below :
"The function block ais is define in power lib and power generation lib"
and on the CM error on the related library (AIS) :
![]()
Could please advise how to solve this library issue ?
or is it need to re-installed/repaired library extension?
Thanks
BR
frisal
I have issue on 800xA system v5.0 that Power Lib 3.0.0 and Power Generation Lib 1.0.0 in Function Block AIS and ais, has an issues when compile the existing project.
Both library is protected so no change / modification on both library.
But the issue pop up on existing logic like below :
and on the CM error on the related library (AIS) :
Could please advise how to solve this library issue ?
or is it need to re-installed/repaired library extension?
Thanks
BR
frisal
Voted best answer
When you Declare the Function Block ( In the declaration pane at the top of your control builder window ) you need to Include the Library Name Eg "Power Lib.AIS" or "Power Generation Lib.AIS"
The FBD code should then also display the <Library> Dot <Function Block > name and the compiler will be able to recognize which FB you are using.
This seems to be a bug in your version of 800xA . Certainly in later versions this happens automatically.
The FBD code should then also display the <Library> Dot <Function Block > name and the compiler will be able to recognize which FB you are using.
This seems to be a bug in your version of 800xA . Certainly in later versions this happens automatically.
Answers
Hi Deepa,
i attached some pic for reference
i attached some pic for reference
Hi,
it seems like ais function block is present in Power Lib and Power Generation Lib either change the name of the function block or else need to delete the block.
it seems like ais function block is present in Power Lib and Power Generation Lib either change the name of the function block or else need to delete the block.
by Deepak.S Rank: 17 on 7/9/2020 9:55:45 PM | Like (0) | Report
Share some screenshot if possible
by frisal.argha-kusumah Rank: 566 on 7/9/2020 10:05:49 PM | Like (0) | Report
hi deepa, please find my pic attached on new comment below
Add new comment